开发、编译、部署
This content is not available in your language yet.
开发、编译、部署
Section titled “开发、编译、部署”以aimdk_examples为例, 合理的目录结构和文件命名如下:
aimdk_examples/├── config/ # 配置文件目录│ └── aimdk_examples/ # 模块配置和数据文件│ ├── BUILD # Bazel 构建文件│ ├── aimdk_examples_config.yaml # 模块运行配置│ └── ... # 其他配置文件│├── scripts/ # 启动脚本目录│ ├── aimdk_examples/ # 模块名目录│ │ ├── BUILD│ │ └── start_aimdk_examples.sh # 模块启动脚本│ └── ... # 其他脚本│├── src/ # 源代码目录│ ├── app/ # 应用程序入口│ │ ├── xxx/ # 具体应用模块│ │ │ ├── BUILD│ │ │ └── main.cc # 主函数入口文件│ │ └── ...│ ││ └── module/ # 模块实现│ ├── xxx/ # 具体功能模块│ │ ├── BUILD│ │ ├── xxx_module.cc # 模块实现文件│ │ ├── xxx_module.h # 模块头文件│ │ └── ... # 其他相关文件│ └── ...│├── tools/ # 工具脚本目录│ ├── build_module.sh # 模块编译脚本│ └── run_module.sh # 模块运行脚本│├── WORKSPACE # Bazel 工作空间配置├── .bazelrc # Bazel 运行时配置├── .bazelversion # Bazel 版本锁定├── .clang-format # 代码格式化规则├── .gitignore # Git 忽略规则└── README.md # 项目说明文档以aimdk_examples模块为例 配置相关 config/aimdk_examples/BUILD
load("@integration//rules/utils:pkg_lib.bzl", "pkg_lib")package(default_visibility = ["//visibility:public"])
filegroup( name = "aimdk_examples_config", srcs = glob(["*.yaml","*.conf"]),)
pkg_lib( name = "aimdk_examples_config_tar", srcs = [ ":aimdk_examples_config", ],)启动脚本相关
Section titled “启动脚本相关”scripts/aimdk_examples/BUILD
package(default_visibility = ["//visibility:public"])
filegroup( name = "aimdk_examples_script", srcs = [ "start_aimdk_examples.sh", ],)src/app/BUILD
load("@rules_pkg//pkg:mappings.bzl", "pkg_attributes", "pkg_filegroup", "pkg_files")load("@rules_pkg//pkg:pkg.bzl", "pkg_tar")load("@integration//rules/utils:flattern_tar.bzl", "flatten_tar")
package(default_visibility = ["//visibility:public"])
cc_binary( name = "aimdk_examples", srcs = [ "main.cpp", ], deps = [ "//src/module/ik:ik_module", "@sdk//:libaimrt", "@sdk//:libaimrt_comm", ],)
pkg_files( name = "aimdk_examples_script", srcs = [ "//scripts/aimdk_examples:aimdk_examples_script", ], attributes = pkg_attributes( mode = "0755", ), prefix = "scripts/aimdk_examples",)
pkg_filegroup( name = "aimdk_examples_filegroup", srcs = [ ":aimdk_examples_script", ],)
pkg_tar( name = "aimdk_examples_without_bin_tar", srcs = [ ":aimdk_examples_filegroup", ], extension = "tar", mode = "0755", tags = ["tar"],)
pkg_tar( name = "aimdk_examples_bin_tar", srcs = [ ":aimdk_examples", ], extension = "tar", include_runfiles = True, mode = "0755", tags = ["tar"],)
flatten_tar( name = "aimdk_examples_bin_flatten_tar", src = ":aimdk_examples_bin_tar", prefix = "bin",)module代码相关
Section titled “module代码相关”load("@integration//rules/utils:header_utils.bzl", "cc_library_with_top_header")
package(default_visibility = ["//visibility:public"])
cc_library( name = "ik_module", srcs = glob([ "*.cpp", ]), hdrs = glob([ "*.h", ]), includes = [".."], deps = [ "@sdk//:libaimrt_comm", ],)单模块完整包相关
Section titled “单模块完整包相关”BUILD
load("@rules_pkg//pkg:pkg.bzl", "pkg_tar")load("@rules_pkg//pkg:mappings.bzl", "pkg_files")load("@integration//rules/utils:patchelf_tar.bzl", "patchelf_tar")
package(default_visibility = ["//visibility:public"])
pkg_tar( name = "aimdk_examples_tar", srcs = [ ], extension = "tar", mode = "0755", strip_prefix = ".", tags = ["tar"], include_runfiles = True, deps = [ "//config/aimdk_examples:aimdk_examples_config_tar", "@integration//:all_plugins_tar", "//src/app:aimdk_examples_bin_flatten_tar", "//src/app:aimdk_examples_without_bin_tar", ],)编译后在bazel-bin中生成aimdk_examples_tar.tar包,包含模块运行所需binary及其依赖so、配置和脚本,解压后包结构: bazel-bin/aimdk_examples_tar
├── bin│ ├── aimdk_examples│ ├── aimrt_main│ ├── iox-roudi│ ├── ...│ ├── libiceoryx_binding_c.so│ ├── libiceoryx_hoofs.so│ └── ...├── config│ └── aimdk_examples│ ├── aimdk_examples_config.yaml│ ├── ...└── scripts └── aimdk_examples └── start_aimdk_examples.sh本地构建工具
Section titled “本地构建工具”在 aimdk_examples 中提供统一的模块构建脚本 tools/build_module.sh,用于本地编译和构建模块。
#!/bin/bashset -e
# Display help information for script usageUsage() { cat <<EOF build_moudle.sh [options] -t: build target module name -c: clean the local bazel cache -a: build with the arch type(x86_64, orin_aarch64), default is x86_64 -j: specify the number of concurrent jobs to run during the build process -g: build with '--copt=-g' -e: extra options -h: help e.g. build_module.sh -t aimdk_examples -a x86_64 -j 8 -g -e "--config=xxx --define=xxx=xxx"EOF exit 1}
# Parse command line arguments using getoptARGS=$(getopt -o a:chgt:j:e: --long arch:,clean_cache,help,debug,target:,jobs:,extra_options: -n "$0" -- "$@")if [ $? != 0 ]; then Usagefi
# Helper function to get formatted timestamp for loggingfunction get_time() { local time=$(date "+%H:%M:%S") echo "($time)"}
# Process parsed argumentseval set -- "${ARGS}"echo $(get_time) INFO: formatted parameters=[$@]
# Initialize default valuesARCH_TYPE="x86_64"BUILD_TARGET=""
# Process command line optionswhile true; do case "$1" in -a | --arch) echo "$(get_time) INFO: Building for arch type: $2" ARCH_TYPE=${2} shift 2 ;; -j | --jobs) echo "$(get_time) INFO: Building using jobs: $2" JOBS_OPTIONS="--jobs=$2" shift 2 ;; -e | --extra_options) echo "$(get_time) INFO: Building with extra options: $2" EXTRA_OPTIONS=${2} if [[ $EXTRA_OPTIONS == *"--config=source"* ]]; then CONFIG_SOURCE="--config=source" fi shift 2 ;; -g | --debug) echo "$(get_time) INFO: Building in debug mode" GDB_FLAG="--copt=-g --copt=-O0" shift ;; -c | --clean_cache) echo "$(get_time) INFO: Building with cleaning cache first" CLEAN_CACHE_FLAG=true shift ;; -t | --target) echo "$(get_time) INFO: Build target" BUILD_TARGET=${2}_tar shift 2 ;; --) shift break ;; -h | --help) Usage ;; *) Usage ;; esacdone
# Validate required target parameterif [ -z "$BUILD_TARGET" ]; then echo "$(get_time) ERROR: Target must be specified, please use -t parameter" Usagefi
# Main build function that executes bazel build commandbuild_module() { target=$1 SHELL_FOLDER=$(cd "$(dirname "${BASH_SOURCE[0]}")" && pwd) pushd "$SHELL_FOLDER"/../ || exit set -x bazel build \ ${COMPILER} \ ${GDB_FLAG} \ ${JOBS_OPTIONS} \ ${EXTRA_OPTIONS} \ "${target}" set +x popd || exit}
# Configure compiler settings based on target architectureif [[ "x$ARCH_TYPE" == "xx86_64" ]]; then COMPILER="--config=x86_64"elif [[ "x$ARCH_TYPE" == "xorin_aarch64" ]]; then COMPILER="--config=orin_aarch64"else echo "$(get_time) ERROR: Unsupported ARCH_TYPE for ${ARCH_TYPE}" exit 1fi
# Clean bazel cache if requestedif [ "${CLEAN_CACHE_FLAG}" == true ]; then set -x bazel clean --expunge || true set +xfi
build_module ${BUILD_TARGET}脚本使用: build_module.sh -t aimdk_examples -a x86_64 -j 8 -g -c -e “—config=xxx —define=xxx=xxx” 参数解释:
- -t: 指定编译模块的名字, 必选
- -a: 执行模块的架构类型,默认为x86_64,可选值为:x86_64和orin_aarch64, 可选
- -j: 指定编译使用的线程数,默认值为0,表示会自动根据当前PC负载动态调整线程数,可选
- -g: 是否编译成调试版本,可选
- -c: 编译前是否清除之前的编译缓存, 可选
- -e: 可以指定额外的编译选型,如—config参数,—define参数等等
本地运行工具
Section titled “本地运行工具”在 aimdk_examples 中提供统一的模块运行脚本 tools/run_module.sh,用于在 AIMDE 环境中运行 x86 架构的模块。
#!/bin/bashset -e
# Function to display usage informationUsage() { cat <<EOF run_module.sh [options] -t: run target module name -c: config file absolute path, default file is in bazel-bin/"\$module_name"_tar/config/"\$module_name"/running_"\$module_name"_cfg.yaml -p: debug port -g: run with debug mode -h: help e.g.: 1) run_module.sh -t aimdk_examples -c config/aimdk_examples/aimdk_examples_config.yamlEOF exit 1}
# Parse command line argumentsARGS=$(getopt -o t:c:p:gh --long target:,config:,port:,debug,help -n "$0" -- "$@")if [ $? != 0 ]; then Usagefi
# Get current timestamp for loggingfunction get_time() { local time=$(date "+%H:%M:%S") echo "($time)"}
eval set -- "${ARGS}"echo $(get_time) INFO: formatted parameters=[$@]
# Initialize variablesRUN_TARGET=""PORT=6215
# Process command line optionswhile true; do case "$1" in -t | --target) echo "$(get_time) INFO: Run target: $2" RUN_TARGET=${2} shift 2 ;; -c | --config) echo "$(get_time) INFO: Run with config: $2" CONFIG_PATH=${2} shift 2 ;; -g | --debug) echo "$(get_time) INFO: Run with debug mode" DEBUG_FLAG=true shift ;; -p | --port) PORT=${2} shift 2 ;; --) shift break ;; -h | --help) Usage ;; *) Usage ;; esacdone
# Validate required parametersif [ -z "$RUN_TARGET" ]; then echo "$(get_time) ERROR: Target must be specified, please use -t parameter" Usagefi
# Store current directory and change to script locationSHELL_FOLDER=$(cd "$(dirname "${BASH_SOURCE[0]}")" && pwd)pushd "$SHELL_FOLDER"/../ || exit # Setup paths and check target existence MODULE_TARGET_TAR_PATH="bazel-bin/${RUN_TARGET}_tar.tar" if [ ! -f "$MODULE_TARGET_TAR_PATH" ]; then echo "$(get_time) ERROR: Target tar does not exist: $MODULE_TARGET_TAR_PATH, please run build_module.sh to build the target tar first" exit 1 fi
# Prepare target directory and extract files rm -rf bazel-bin/${RUN_TARGET}_tar || true mkdir -p bazel-bin/${RUN_TARGET}_tar tar -xvf "$MODULE_TARGET_TAR_PATH" -C bazel-bin/${RUN_TARGET}_tar
# Prepare execution command EXEC_SHELL_SCRIPT_PATH="bazel-bin/${RUN_TARGET}_tar/scripts/${RUN_TARGET}/start_${RUN_TARGET}.sh" chmod a+x ${EXEC_SHELL_SCRIPT_PATH} EXEC_COMMAND="${EXEC_SHELL_SCRIPT_PATH}"
# Add optional parameters to command if [ -n "$CONFIG_PATH" ]; then EXEC_COMMAND+=" -c ${CONFIG_PATH}" fi if [ -n "$DEBUG_FLAG" ] && [ -n "$PORT" ]; then EXEC_COMMAND+=" -g -p ${PORT}" fi
# Execute the command ${EXEC_COMMAND}popd || exit脚本使用: run_module.sh -t aimdk_examples -c config/aimdk_examples/aimdk_examples_config.yaml 参数解释:
- -t: 指定编译模块的名字, 必选
- -c: 指定配置文件的绝对路径,如何未指定,使用打包后默认的配置文件, 可选
- -g: 是否启动调试模式,可选
- -p:指定调试端口,默认值为6125, 可选
编译单模块包
Section titled “编译单模块包”针对目标芯片架构编译模块:
bash tools/build_module.sh -t aimdk_examples -a orin_aarch64 # ARM架构(Orin)# 或bash tools/build_module.sh -t aimdk_examples -a x86_64 # x86架构部署到目标设备
Section titled “部署到目标设备”传输编译产物
Section titled “传输编译产物”将编译生成的tar包传输至目标设备:
sshpass -p 1 scp \ -o UserKnownHostsFile=/dev/null \ -o StrictHostKeyChecking=no \ -o ConnectTimeout=120 \ -P 61120 \ /workspaces/aimde/aimdk_examples/bazel-bin/aimdk_examples_tar.tar \ agi@192.168.111.140:/agibot/data/home/agi/ggm/登录设备并解压
Section titled “登录设备并解压”登录Orin板:
ssh agi@IP -p 61120解压并清理安装包:
Section titled “解压并清理安装包:”cd /agibot/data/home/agi/ggm/tar -xvf aimdk_examples_tar.tarrm -rf aimdk_examples_tar.tar进入部署目录并启动服务:
cd /agibot/data/home/agi/ggm/bash scripts/aimdk_examples/start_aimdk_examples.sh